{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can an ATS22 softstart be used on an ungrounded delta system?
Issue:
Running an ungrounded delta system with an ATS22.

Product Line:
Altistart 22, ATS22

Environment:
All

Cause:
N/A

Resolution:
Yes, the ATS22 can be used on an ungrounded delta system as long as the line voltages are balanced phase to phase (L1, L2 and L3).

Schneider Electric Global