{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I change the Min and Max frequency range displayed on the bottom of the keypad when in local (HMI) mode on the ATV630 Process drive?
Issue:
Frequency range displayed adjustment in local mode for process drives.

Product Line:
ATV630 Process drive

Environment:
All models and serial numbers

Cause:
Wants to display operator range.

Resolution:
In HMI (local) mode, the display shows at the bottom -500Hz to +500Hz.  There is not a way to change these values.
The drive was designed to show the complete range of the drive.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global