{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you set up the AI2 analog input for Ref 1 channel on the ATV61 and ATV71 drives?
Issue:
Trying to set up the AI2 analog input for the Ref 1 channel on the ATV61 and ATV71 drives.

Environment:
All

Cause:
Wants to set up the ATV61 drive so that it uses the 4 to 20mA  on AI2's input for the speed reference on ref 1 channel.

Resolution:
Go into 1.6 menu  (Command menu):  Set Ref 1 channel to be AI2.  Note: On the ATV61, Ref 1 B channel is default set to AI2.  If you are not in expert or Advanced setup mode, you will need to unassign the Ref 1 B channel 1st in the menu 1.7 application function and then change the Ref 1 channel, under menu 1.6 to AI2.

Schneider Electric Global