{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a MFH / MF1 CT (Current Transformer) for Easergy Flair be installed on a RMU, having two single core cables per phase?

1.1 - Application

This FAQ is applicable when it is required to install  MFH / MF1 CT (Current Transformer) on RMU having two single core cables per phase.

1.2 - Solution

The solution is to install two MFH / MF1 CT per phase on each single core cable as per below picture. These CTs have to be installed as specified in the RMU documentation, with cable shielding going back through each phase. Secondary of CTs on the same "phase" have to be connected in parallel for each CT input of FPI. No summation CT is required here. This solution with 2 MFH / MF1 CTs per phase has been implemented at different sites globally.

1.2 - Performance

Since MF1 CT is installed  parallelly on two cables of each phase, each cable will be  well centered inside the CT, hence accuracy loss will be almost negligible. This is not advisable in case of MFH Zero Sequence CT, because the cables will not be centered on CT. Hence this can affect the accuracy.

Schneider Electric Global

Attachment(s)
FAQ_CT connection.pdf [149.28 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.