{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why a bandwidth limitation on the service port of 140NOC78xxx?
Issue

Why do we have a limitation on the service port of a 140NOC78x00?

Product Line

Quantum

Resolution

Servicing the service port (low priority) slows down the process of servicing the control port (high priority); to resolve the latency that can be caused by the traffic from the service port toward the traffic on the control port, a limitation is set on the service port.

Schneider Electric Global