{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
When using a USOPTL4 (RS485-USB adapter) in Power Monitoring Expert the serial site times out, however Modbus Tester can successfully connect to the adapter
Issue
Customer has a daisy chain connected serially to the computer using RS485-USB adapter (Model#: USOPTL4). He can connect to any meter on that daisy chain and read registers using Modbus Tester (See FA180037 to learn more about Modbus Tester). However when using the adapter as a serial site in PME, the connection times out.

Product Line
RS485-USB adapter (Model#: USOPTL4)

Environment
ION Enterprise 6.0 SP1
StruxureWare Power Monitoring 7.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Modbus Tester

Resolution
Modbus Tester software requires the "Echo" dip switch (located on the back of RS485-USB adapter) to be ON when communicating with Modbus devices.
Power Monitoring Expert, StruxureWare Power Monitoring, and ION Enterprise require "Echo" to be OFF when communicating with devices.
ION Setup 3.0 configuration software also requires "Echo" to be OFF.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.