undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to use PSE to control PM5350’DO via PwrModubs protocol
1. First using PM5350 to control we need to write 3 register together. If we want to send command to DO1 to  we need to write 5250=6003,5251=0 and 5252=1 and send  the frame  like :01 10 14 81 00 03 06 17 73 00 00 00 01 XX XX. (XX XX is for CRC).

2. We can use the block writes to write multiple registers. By using fixed block writes follow the format below:
Fixed block writes have the following format:
T:BWF;[D:{B|C|M|P};]S:<start_register>,<values>
where
B, C, M, or P are applicable only to Micrologic devices (otherwise the D: section
is omitted) and is the module (manager) identifier (Circuit Breaker, Chassis,
Metering, Protection).
<start_register> is the first register number for a contiguous block of registers.
<values> is a comma-separated list of up to 10 values that will be written to the
registers starting from <start_register>.
For PM5350 control tag looks like T:BWF;S:5250,6003,0,1 and this tag must be DIGITAL. By setting this tag to 1 to make it works.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.