Video: When to use the Internet Explorer Browser object in Vijeo Designer
Published date:
21 February 2019
Issue:
When to use the Internet Explorer Browser object in Vijeo Designer
Product Line:
Magelis iPC or HMI targets running Windows Operating Systems
Resolution:
The Internet Explorer browser object in Vijeo Designer is only to be used with iPC or HMI targets running Windows Operating Systems. When using this object in a Windows environment, you will be able to open web pages as you would on your regular PC within the Vijeo Designer Runtime window.
When using HMIs such HMISTU, HMISTO, XBTGT, XBTGK, HMIGTO, HMIGTU, use the Multi-platform Browser Object instead. This object will allow you to open pre-downloaded files such as HTML that you include at Data Files node in Vijeo Designer.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.