{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What is the range of wavelength acceptable by ACE937 module?

Issue
Specification needed for ACE937 input

Product Line
ACE937

Environment
Sepam 20, 40, 80

Resolution
ACE937 fiber optic interface can accept a minimum wavelength of 792 nm and maximum wavelength of 865 nm. The most common wavelength, as shown in the manual, is 820 nm.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: