Browse FAQs

Can the 140CFA04000 Cablefast block be used with the 140ATI03000 module?

Published date: 04 November 2019

Issue:
Using Cablefast with a Quantum Thermocouple card.

Product line: 
Quantum Cablefast system

Cause:
Fluctuation in readings using the Cablefast solution.

Resolution:
The 140CFA04000 block does not incorporate an isometric barrier and is not
recommended for use with the 140ATI03000 TC module. Without such a barrier,
temperature readings may vary up to 2 degrees from one end of the block to the
other. If the application can tolerate this temperature error, the block (and module
remote CJC) may be used.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.