Browse FAQs

Setting up permissive function on the ATV61 and ATV71 drives?

Published date: 26 December 2019

Issue:
On the ATV61 and ATV71 drives how can you add another run permissive input if you already have freewheel stop assigned?

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
There are several options of adding another run permissive on this drive.
- You can remove the factory jumper and tie in your stop circuit between the PWR and +24 terminals
- You can assign a Fast Stop as a logic input
  - Drive Menu ~> 1.7 Application Function Menu ~> Stop Configuration ~> Fast Stop Assignment
- You can use an External Fault with either Normally Closed or Normally Open set of contacts
  - Drive Menu ~> 1.8 Fault Management Menu ~> External Fault ~> External Fault Assignment

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.