{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Sepam 80 - is it possible to order spare plastic connectors for the MES120 module?
Yes.  In the 2014 edition of the Sepam 80 "Operation" user manual, the reference given refers to the MES114 instead of the MES120.

The reference 59676 does indeed refer to the "Kit 2640" which includes 2 sets of the 3 plastic connectors that are required for each MES120 module.


AEDL3

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.