Browse FAQs

Is there a preassembled cordset with flying leads to use with the BMXDDI6402K module besides using the Telefast module?

Published date: 16 May 2018

Issue:
Is there a preassembled cordset with flying leads to use with the BMXDDI6402K module besides using the Telefast module?

Product Line:
M340, X80, Telefast

Resolution:
Yes, you can use the preassembled cordset with flying leads for the BMXDDI6402K.  Below are the part numbers:
BMXFCW303  (3m)
BMXFCW503  (5m)
BMXFCW1003  (10m)

You will need a quantity of 2 as these cordset are 2 x 20, 40 way connectors.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.