Browse FAQs

What will cause a CLr fault on the ATV212?

Published date: 09 December 2019

Issue: 
Getting a CLr fault on the ATV212.

Product Line:
ALTIVAR 212

Environment:
All models
 
Cause:
Troubleshooting

Resolution:
CLr [Reset active] is a status which is displayed after the STOP/RESET key is pressed while a detected fault is displayed. It indicates that the cause of the detected fault has cleared and the fault status can be reset. Press the STOP/RESET key again to clear the detected fault.  This type of fault reset only applies when in Local mode or in Remote mode with CMOd=1 ( HMI ).  It also only applies to the following faults:

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.