{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you set the current limit on the ATV61 and ATV71 drives?
Issue:
Setting the current limit on the ATV61 and ATV71 drives

Product Line:
Altviar ATV61 and ATV71 drives

Environment:
All

Cause:
Wants to set up the current limit setting on the drive.

Resolution:
From the Main menu, go into the Drive Menu
Scroll down to the 1.4 motor control menu and press Enter
Select Current Limit, press Enter, and set your current limit value.
The default current limit values will be set to 1.10 X the ATV61 Drives' current ratings and 1.50 X the ATV71 Drives' current rating.

Schneider Electric Global