Browse FAQs

My ATV312 drive will not change from local to remote mode by holding the Mode button.

Published date: 23 October 2019

Issue:
Cannot change from Local to Remote on my ATV312 drive, by holding the Mode button.

Product Line:
ATV312 series drives

Environment
Firmware version 5.1 IE56 and above.

Cause:
Recent firmware change.

Resolution:
As of firmware version 5.1 IE56, The ATV312 series drives can no longer be switched from local mode to remote.  In order to change the drive from local to remote, you perform a factory reset using the FCS parameter.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.