Browse FAQs

Can the TMH2GDB display floating point numbers?

Published date: 11 November 2019

Issue:
Limitations of the TMH2GDB Remote Graphic Display

Product line:
M221 all supported PLC's

Environment:
Remote Graphic Display

Cause:
Limitations on the Remote Graphic Display for reading data.

Resolution:
No. The TMH2GDB does not support floating point. The following Object Types are supported. 
These memory objects are available:
 System bit (%S)
 System word (%SW)
Memory bit (%M)
Memory word (%MW)
Constant word (%KW)
Memory double word (%MD)

These I/O objects are available:  
Input bit (%I)
Output bit (%Q)
Input word (%IW)
Output word (%QW)
Input status word (%IWS)
Output status word (%QWS)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.