Browse FAQs

Unable to uninstall Vijeo Designer

Published date: 23 October 2019

Issue:
Error 1500: "Another installation is in progress" error appears when trying to uninstall Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
This error is not a problem specifically with Vijeo Designer software itself. It is however an issue with your Windows Installer service in your Windows operating system. To resolve this issue, please follow this procedure:

1) Goto the Control Panel and open the Adminstrative Tools
2) Open the Services 
3) Find the Windows Installer Service and disable it.
4) Reboot the PC
5) Go back to find the Windows Installer Service and re-enable it
6) Once it is renabled, re-start the Windows Installer Service

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.