What are the part numbers for the PM8000 accessories and parts?
Published date:
14 March 2019
Product Line
PM8000 meter series
Environment
Part number, commercial reference
Resolution
Part Number
Description
METSEPM8240
Intermediate metering with class 0.2S accuracy + 3 digital status/counter inputs + 1 KY(form A) energy pulse output & dual port ethernet + serial communications. PM8000 power meter panel mount with display.
METSEPM8210
Same as the PM8240, except with low-voltage DC control power
METSEPM82401
Same as the PM8240, except the meter is calibrated to comply to MID standards
METSEPM82403
Same as the PM8240 with the addition of a sealable hardware lock which prevents modification of revenue related settings and functions.
METSEPM82404
Same as the PM82403 except that it is sealed at the factory.
METSEPM8243
Intermediate metering with class 0.2S accuracy + 3 digital status/counter inputs + 1 KY(form A) energy pulse output & dual port ethernet + serial communications. PM8000 power meter din rail no display.
METSEPM8213
Same as the PM8243, except with low-voltage DC control power
METSEPM8244
Intermediate metering with class 0.2S accuracy + 3 digital status/counter inputs + 1 KY(form A) energy pulse output & dual port ethernet + serial communications. PM8000 power meter din rail with remote display.
METSEPM8214
Same as the PM8243, except with low-voltage DC control power
METSEPM89RD96
ION7400 / PM8000 REMOTE DISPLAY WITH 3M CABLE
METSEPM89M2600
ION7400 / PM8000 DIGITAL I/O MODULE, 2 RELAY, 6 DIGITAL INPUTS
METSEPM89M0024
ION7400 / PM8000 ANALOG I/O MODULE, 2 OUT, 4 IN
METSEPM8000SK
ION7400 / PM8000 SEALING KIT
METSEPM8HWK
ION7400 / PM8000 POWER METER HARDWARE REPLACEMENT KIT (5 connectors, 2 mounting brackets, 4 CT screws)