Browse FAQs

PM5000 LE driver for ION enterprise 6.0 SP1

Published date: 29 January 2019

Issue
PM5000 series meters are not native supported on ION Enterprise 6.0 SP1 software. 

Product Line
PM5000 series meters

Environment
ION Enterprise 6.0 SP1

Resolution
LE driver for PM5000 meters on ION Enterprise 6.0 SP1 attached to this article: Note: ION Enterprise 6.0 SP1 is no longer supported.

Run the "PM5000 LE 6.0.1.11 Driver Setup.exe" file inside the zip, and follow the installation process.  Once completed, The PM5000 series LE will be available when adding the device in the Management Console as a Device Type.  Add the PM5000 and verify connection.  If the newly added PM5000 meter values are not showing on Vista, perform a server restart.  


NOTE: this driver is a LE (Limited Edition) driver. The LE driver supports all real time data registers, default PC logging but doesn't support retrieval of onboard logs or any digital output control operations. The PM5000 series meter is fully supported on the newer version of the software, Power Monitoring Expert 8.2 and later.

Kindlt refer to the link below for more information:

https://www.se.com/ww/en/product-range-presentation/62919-ecostruxure%E2%84%A2-power-monitoring-expert​

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.