{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does Control Expert (formerly Unity Pro) offer a way to detect if an ERIO drop has a problem on one or more of its IO modules?
Yes, the following System Words can be used to determine module health in an ERIO drop.

%SW152-153  Referred to as ERIO_Drop_Status
0=There is a problem with one or more modules in this drop
1=Drop status is good, no IO problems in this drop


R-71317

Schneider Electric Global