{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PME error "failed to write node info to database because 'The server threw an exception. (Exception from HRESULT - 0x80010105 (RPC_E_SERVERFAULT))'

Issue:
A customer is seeing the following error message within the System Log events.

"failed to write node info to database because 'The server threw an exception. (Exception from HRESULT - 0x80010105 (RPC_E_SERVERFAULT))'. Will retry in 60s.)"

Product Line:

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x



Environment:
Windows server 2008

Windows server 2008 R2

Windows server 2012

Windows server 2012 R2

Cause:
The system has corrupt operating system files.

Resolution:
The system will require either formatting and restoring from back ups or installation on a new machine.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: