Issue:
ATV320 using full motor torque at zero speed.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
To run the drive in a closed loop mode
Resolution:
The Altivar 320 is very similar to Altivar 32 and the Altivar 312.
All of these products do not manage closed loop regulation.
For closed loop control, consider an Altivar 71 or Altivar 900 series drive plus an encoder option card.
ATV320 using full motor torque at zero speed.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
To run the drive in a closed loop mode
Resolution:
The Altivar 320 is very similar to Altivar 32 and the Altivar 312.
All of these products do not manage closed loop regulation.
For closed loop control, consider an Altivar 71 or Altivar 900 series drive plus an encoder option card.
Released for:Schneider Electric Global
Issue:
ATV320 using full motor torque at zero speed.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
To run the drive in a closed loop mode
Resolution:
The Altivar 320 is very similar to Altivar 32 and the Altivar 312.
All of these products do not manage closed loop regulation.
For closed loop control, consider an Altivar 71 or Altivar 900 series drive plus an encoder option card.
ATV320 using full motor torque at zero speed.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
To run the drive in a closed loop mode
Resolution:
The Altivar 320 is very similar to Altivar 32 and the Altivar 312.
All of these products do not manage closed loop regulation.
For closed loop control, consider an Altivar 71 or Altivar 900 series drive plus an encoder option card.