Issue:
How is language changed on the remote HMI connected to the ATV212?
Product Line:
Altivar 212
Environment:
All models
Cause:
Preferred language is different than current setting
Resolution:
The ATV212 integral display provides code, therefore language is not an issue. However, the remote LCD keypad, VW3A1101, provides descriptive readout. If the language needs to be changed, either power up the VFD with the keypad connected, or connect the keypad to a powered VFD. The HMI will initialize itself. When it reaches the Main Menu, there is selection for Drive Menu and Language. Quickly scroll to Language and select it. A list of available languages will be appeared for selection.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.