{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
On an ATS48, what functions are available for the logic outputs?
Issue:
ATS48 available functions for the logic outputs.

Product line:
ATS48, Altistart 48

Environment:
All

Cause:
N/A

Resolution:
Default assignment for LO1 is Motor thermal alarm, tAl. Default assignment for LO2 is motor powered, rnl.
Available assignments are:
- no - not assigned
- tAl - Motor Thermal alarm
- rnl - motor powered
- AIL - motor current alarm
- AUL - motor underload alarm
- APC - motor PTC probe alarm
- AS2 - second set of motor parameters activated.

Schneider Electric Global

Attachment(s)
ATS48 LO assignments.bmp [1.85 MB]