{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Link150 Password Reset
Issue
It is not possible to generate the backdoor password of Link150. We have to perform only the factory reset so Link150 will return to the default user name and password.
Product Line
Link150

Cause
Forgetting the web page password for the Link150

Resolution
Module State Indication LED shall flash, GREEN for first 10 seconds, and then RED for 10-15 seconds.
ActionsEffects
Press and hold the 'reset pin' 1 - 5 seconds LED: Flashing GREEN
10 - 15 seconds LED: Flashing RED: All user-configurable information is reset to factory defaults


Release the pin when the Module State LED starts flashing RED (i,e 10 - 15 seconds)    Device reboots.
Factory settings will be applied. The default password can be found at FA299649

NOTE:
•    If the 'reset pin' is released, after 5 seconds and before 10 seconds, no action will be performed, LED will be flashing GREEN, till the 'reset pin' is released.
•    If the 'reset pin' is released after 15 seconds, no action will be performed, LED will be turned to GREEN.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.