{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are errors E1300 and E1301 on the LXM32 drive?
Issue:
Errors E1300 and E1301 on the LXM32 drive

Product Line:
LXM32

Resolution:
E1300 means a safety STO function is activated (STO_A, STO_B)
E1301 means the levels of the inputs STO_A and STO_B were different for more than 1 second
These 2 errors are related to a bad wiring of inputs STO_A and STO_B, a bad 24V power supply or an activated emergency stop, which cuts the 24VDC from the STO inputs.
Making sure the STO inputs are getting 24VDC before powering the drive will reset these faults.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: