Browse FAQs

What could be one of the reason why I can't put my M258 controller into Run mode using SoMachine V4.3

Published date: 04 September 2018

I get the following error when trying to put my M258 Controller in run mode.

SoMachine is unable to start the controller. Be sure that the Run/Stop input is enabled. (Set to Run).



Check to see if the Run/Stop input has been configured. If it is then the associated input must be True to put the controller into Run mode.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.