Does Schneider Electric offer motor type BDM4564S0115 ?
Published date:
16 September 2019
No, the motor type BDM4564S0115 is a customized version of Brushless DC motor which has special design features unique for the OEM machine builder that uses this model.
This model is proprietary for the OEM machine builder and the sale of this model is restricted to only the OEM.
Customers looking for BDM4564S0115 must contact the OEM machine builder to get spares.
rev 9-16-19
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.