{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I clone an application from a Magelis HMI to another unit with a USB flash drive?
Issue:
Looking for a way to move a program from one HMI to another HMI

Product Line:
Vijeo Designer, Magelis, Harmony

Resolution:
The Magelis HMI does not have cloning capability with a USB Flash drive.

The application must be transferred first from Vijeo Designer to the USB Flash Drive or CF / SD card (File System transfer) in order to load the application to a new Magelis.

Schneider Electric Global