Can PM5300 data be accessed using a built-in webpage through its Ethernet port?
Published date:
01 February 2019
Issue
Can PM5300 data be accessed using a built-in web page?
Product Line
PM5300
Environment
HTTP server. Webpage access
Resolution
PM5300 does not have HTTP server and it does not have built-in webpages saved on its memory. Therefore, its data can't be accessed using this method.
The data is still accessible by reading Modbus registers through its Ethernet port.
PM5000 register list can be downloaded from FA234017
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.