{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number of the extended I/O option card for ATV61 and ATV71 drives?
Issue:
Part number of the extended I/O option card for ATV61/71 drives.

Product Line:
ATV61, ATV71

Environment:
All

Cause:
Additional I/O

Resolution:
The part number is VW3A3202.
Contains all the I/O on the basic I/O option card (VW3A3201; 4 logic inputs, 2 logic outputs, 1 form C relay output, an input for PTC motor probes, a 24Vdc output, and a 10VDC output) with additional 2 analog inputs, 2 analog outputs, and 1 pulse input.

Schneider Electric Global