Issue:
What are the part numbers for the M221 connectors.
Product line:
TM221
Cause:
Either missing connectors or need connectors to wire up before the system arrives for install.
Resolution:
TMAT2CSET - connector set for M221C - IO
TMAT2MSET - connector set for M221M and TM3 - IO
TMAT2MSETG - connector set for M221M and TM3 - IO Spring
TMAT2PSET - connector set for M2X1 - power supply
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.