{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
NetBotz Rack Monitor 250 Sensor Pod and Remote Sensor events missing from “By Event” configuration page

Issue

Sensor Pod and Remote Sensor type events (with the prefix SP or RS) are missing from the Event Actions for Individual Events list on the NetBotz Rack Monitor 250.
Configuration->Notifications->Event Actions-> By Event configuration page:



Excerpt of event list below:


Product Line
  • NetBotz Rack Monitor 250


Environment
  • All serial numbers
  • All firmware versions

Cause

This is a firmware issue. It occurs whether or not there are supported sensor pods (Sensor Pod 150/NBPD0150) or remote sensors (AP9520) connected to the Rack Monitor 250 appliance.


Resolution

Configure sensor pod (SP) and remote sensor (RS) type events by groups rather than by individual event. Navigate to the Configuration->Notifications->Event Actions-> By Group menu option, and apply configurations by Severity or Category.



Alternatively, to configure SP and RS type events individually, use the method explained in knowledge base article ID FA156104, and rely on event code IDs in the text file attachment to this knowledge base.

Schneider Electric Global

Attachment(s)
NB250-SP_RS-eventcodes.txt [4.66 KB]