Title
Archive a Unity applications with remote BMXPRA0100 programs
Issue
Archive a Unity applications with remote BMXPRA0100 programs
Product Line
M340 BMXPRA0100
Environment
Unity Pro
Cause
N/A
Resolution
After your BMXPRA0100 Unity application is configured: (Built and downloaded to the BMXPRA0100)
You need to use the Export or Save Archive function for your BMXPRA0100 application before you Close the BMXPRA0100 application instance of Unity Pro
NOTE: When You are asked if you want to save the PRA application in the master application *.stu file, answer YES.
Then the PRA application is saved (embedded) in the master application. If you select No, all changes are lost.
When sending the application to another person, create a .ZEF copy of the Master M340 application.
Archive a Unity applications with remote BMXPRA0100 programs
Issue
Archive a Unity applications with remote BMXPRA0100 programs
Product Line
M340 BMXPRA0100
Environment
Unity Pro
Cause
N/A
Resolution
After your BMXPRA0100 Unity application is configured: (Built and downloaded to the BMXPRA0100)
You need to use the Export or Save Archive function for your BMXPRA0100 application before you Close the BMXPRA0100 application instance of Unity Pro
NOTE: When You are asked if you want to save the PRA application in the master application *.stu file, answer YES.
Then the PRA application is saved (embedded) in the master application. If you select No, all changes are lost.
When sending the application to another person, create a .ZEF copy of the Master M340 application.
Released for:Schneider Electric Global