Browse FAQs

Are  the ATV600 series drives compatible with Ethernet?

Published date: 01 November 2019

Issue: 
Are  the ATV600 series drives compatible with Ethernet Modbus TCP?

Product Line:
ALTIVAR PROCESS DRIVES

Environment:
All
 
Cause:
Installation 

Resolution
Yes, Ethernet TCP/Modbus TCP is standard integrated functionality.  Ethernet IP requires a separate Option Card VW3A3720 (min. Firmware ver. 1.5) or (min. Firmware ver. 1.6) VW3A3721 These are both combination TCP/IP and Ehternet IP Option Modules with dual port daisychain functionality.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.