Issue
Want to be able to communicate over TCP/IP and was wondering if the old Sepam in the field has the ability.
Product Line
ACE850TP/ ACE850FO
Resolution
The Sepam 40 and Sepam 80 must have a minimum firmware shown in the below table.
Note: That the ACE850 cannot be used with the Sepam 20 series.
Want to be able to communicate over TCP/IP and was wondering if the old Sepam in the field has the ability.
Product Line
ACE850TP/ ACE850FO
Resolution
The Sepam 40 and Sepam 80 must have a minimum firmware shown in the below table.
ACE850 (TP/FO) | Version OK |
Sepam Series 40 | V7.00 or Greater |
Sepam Series 80 | Base & Application V6.00 or Greater |
Note: That the ACE850 cannot be used with the Sepam 20 series.
Released for:Schneider Electric Global