Browse FAQs

Software used to commission the LXM28 or LXM32 servo drive

Published date: 16 October 2019

Issue:
Which software is used to commission the Lexium 28 or LXM32 servo drive?

Product Line:
Lexium 28

Resolution:
The software is SoMove V2.6.2.0 (latest version today). 
Here is a link to download it: 
https://www.se.com/ww/en/download/range/2714-SoMove/?docTypeGroup=3541958-Software%2FFirmware
You first need to install SoMove V2.6 (FDT Standalone) and then install the LXM28 DTM Library (See attached). 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.