{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why do I get a Microsoft Visual C++ 2008 SP1 Redistributable package error when installing SP3.1 Webgate client for Vijeo Designer?
The Microsoft Visual C++ 2008 SP1 Redistributable package was not included with SP3.1

As a workaround you can install the SP3 webgate client file which includes Microsoft Visual C++ 2008 SP1 Redistributable package then install SP3.1.

webgate


Schneider Electric Global