Does Power Monitoring Expert require Adobe Flash Player?
Published date:
21 December 2018
Issue
Can Adobe Flash Player be removed from the server hosting Power Monitoring Expert without negatively affecting the PME software?
Environment
PME 7.2.x, PME 8.x
Resolution
Adobe Flash Player is not required within the Power Monitoring Expert software.
It can be removed without affecting the operation of the software.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.