{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What sizes are available for the Altivar 630 and Altivar 930 Process drive?
Issue:
Sizes for the Altivar 630 and Altivar 930 drives.

Product Line:
Altivar Process Drive (ATV630, ATV930)

Environment:
All serial numbers for ATV630/930 Process Drive

Cause:
N/A

Resolution:

Size 1
  • 208/240Vac
    • 0.75 – 4kW (1 - 5hp)
      • ATV630U07M3, ATV630U15M3,  ATV630U22M3, ATV630U30M3, ATV630U40M3
      • ATV930U07M3, ATV930U15M3,  ATV930U22M3, ATV930U30M3, ATV930U40M3
  • 400/460Vac
    • 0.75 – 5.5kW (1 - 7.5hp)
      • ATV630U07N4, ATV630U15N4, ATV630U15N4, ATV630U22N4, ATV630U30N4, ATV630U40N4, ATV630U55N4
      • ATV930U07N4, ATV930U15N4, ATV930U15N4, ATV930U22N4, ATV930U30N4, ATV930U40N4, ATV930U55N4
Size 2
  • 208/240Vac
    • 5.5kW (7.5hp)
      • ATV630U55M3
      • ATV930U55M3
  • 400/480Vac
    • 7.5 – 11kW (10 - 15hp)
      • ATV630U75N4, ATV630D11N4
      • ATV930U75N4, ATV930D11N4
Size 3
  • 208/240Vac
    • 7.5 – 11kW (10 - 15hp)
      • ATV630U75M3, ATV630D11M3
      • ATV930U75M3, ATV930D11M3
  • 400/480Vac
    • 15 – 22kW (20 - 30hp)
      • ATV630D15N4, ATV630D18N4, ATV630D22N4
      • ATV930D15N4, ATV930D18N4, ATV930D22N4
Size 4
  • 208/240Vac
    • 15 – 22kW (20 - 30hp)
      • ATV630D15M3, ATV630D18M3, ATV630D22M3
      • ATV930D15M3, ATV930D18M3, ATV930D22M3
  • 400/480Vac
    • 30 – 45kW (30 - 60hp)
      • ATV630D30N4, ATV630D37N4, ATV630D45N4
      • ATV630D30N4, ATV630D37N4, ATV630D45N4
Size 5
  • 208/240Vac
    • 30 – 45kW (40 - 60hp)
      • ATV630D30M3, ATV630D37M3, ATV630D45M3
      • ATV930D30M3(C), ATV930D37M3(C), ATV930D45M3(C)
  • 400/480Vac
    • 55 – 90kW (75 - 125hp)
      • ATV630D55N4, ATV630D75N4, ATV630D90N4
      • ATV930D55N4(C), ATV930D75N4(C), ATV930D90N4(C)
Size 6
  • 208/240Vac
    • 55 – 75kW (75 - 100hp)
      • ATV630D55M3, ATV630D75M3
      • ATV930D55M3C, ATV930D75M3C
  • 400/480Vac
    • 110 – 160kW (150 - 250hp)
      • ATV630C11N4, ATV630C13N4, ATV630C16N4
      • ATV930C11N4C, ATV930C13N4C, ATV930C16N4C
Size 7A
  • 400/480Vac
    • 220kW (350hp)
      • ATV630C22N4
      • ATV930C22N4(C)
      • Similar to Frame size 12 for the ATV61/71

Size 7B
  • 400/480Vac
    • 250 – 315kW (400 - 500hp)
      • ATV630C25N4, ATV630C31N4
      • ATV930C25N4C, ATV930C31N4C
      • Similar to Frame size 13 for the ATV61/71
Note:
"C" Suffix means it comes without a braking resistor.



drive atv630

drive size2 atv630

Schneider Electric Global