{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you have Vijeo Design'Air and Vijeo Design'Air Plus connect to the Magelis terminal simultaneously?
Issue:
Can you have Vijeo Design'Air and Vijeo Design'Air Plus connect to the Magelis terminal simultaneously?

Product Line:
Vijeo Designer, VD'Air, VD'Air Plus

Resolution:
The target machine only allows one instance of Vijeo Design'Air or Vijeo Design'Air Plus to access its data at a given time.

For example, if Vijeo Design'Air Plus has an active data sharing connection to the target machine, Vijeo Design'Air cannot establish a remote connection.  If Vijeo Design'Air has a remote connection established, Vijeo Design'Air Plus can still download and launch the project, but it cannot share data with the target machine.

Schneider Electric Global