Browse FAQs

How many simultaneous explicit messaging connections you can have with the BMENOC03x1 as a server?

Published date: 24 October 2019

Issue:
How many simultaneous explicit messaging connections you can have with the BMENOC03x1?

Product Line:
M580
BMENOC0301
BMENOC0311
BMENOC0321

Environment:
Ecostruxure Control Expert
Unity Pro

Resolution:
The BMENOC03x1 can support up to 32 explicit messages as a server for Ethernet/IP or Modbus/TCP.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.