Does Schneider Electric offer motor type BRS397WS0868 ?
Published date:
08 April 2019
No, motor type BRS397WS0868 is an OEM specific model with unique design features for the OEM machine builder that uses this model.
The model is proprietary to the OEM machine builder and is not available directly from Schneider Electric due to a contractual agreement with the OEM
Customer in need of BSR397WS0868 should contact the OEM machine builder for a spare or a replacement.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.