Browse FAQs

What would cause the ATV930 process drive to get a precharge capacitor fault?

Published date: 18 September 2018

Issue:
What would cause the ATV930 process drive to get a precharge capacitor fault?

Product Line:
ATV930 process drives

Environment:
All

Cause:
DC bus tie with another drive

Resolution:
In a configuration where the drive is connected and supplied by another drive via the DC bus, set DCBS parameter (Generic Functions/DC-Bus Ref Link) to "Drive with REC" as shown in the attachment. This will avoid "Precharge Capacitor" faults due to power supplied direct to the DC bus.

[Complete settings] -> [Generic functions] -> [dbS] -> [dCbS] -> [Drive with REC]

More details can be found on page 441 of the ATV900 Programming Manual:
https://www.se.com/ww/en/download/document/NHA80757/

Note: the ATV600 series is not designed for applications where the DC bus is powered from an external DC source.
.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.