What is the pin assignment for Lexium 32 motor cable VW3M5101Rxx ?
Published date:
23 October 2018
Black wire with 1 printed on it should be wired to U on motor connector of drive
Black wire with 2 printed on it should wired to V on motor connector of drive
Black wire with 3 printed on it should be to W on motor connector of drive
Green/Yellow wire is protective ground and it should be wired to PE on motor connector of drive
Note, the brake release wires are only needed for motors with brake.
White wire is brake + and should be connected to BR+ (pin A) on brake connector of drive
Gray wire is brake - and should be connected to BR- (pin B) on brake connector of drive
See attached images for clarification of connector terminals
rev 10-23-18
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.