{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
The XXMIT 'Response Timeout' parameter (RESPSTOUT) does not operate correctly in a Unity Momentum processor.
Issue
This resolution describes the issue that occurred with the RESPSTOUT parameter on the XXMIT Function Block and how the issue is resolved.


If configuring an XXMIT Function Block in a Unity Momentum PLC, the RESPSTOUT parameter value is stuck at 100ms, regardless of the value the user assigns to this parameter.



Product Line
171CBU78090

171CBU98090
171CBU98091


Resolution
A fix for the XXMIT Response Timeout issue will be in Unity 12.

For Unity 11.1, HotFix 'HF UnityPro_V111_HF0347199R' is available. (see attachments)


Schneider Electric Global

Attachment(s)
UnityPro_V111_HF0347199R.zip [6.16 MB]