{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV320 be programmed without power?

Article available in these languages: Czech, Spanish

Issue:
ATV320 Programming without line power

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
Customer wants to program the ATV320 with a Multiloader without line or control voltage connected to the drive.

Resolution:
Yes, the ATV320 can be programmed via the Multiloader with no external power source applied.

Schneider Electric Global