{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you assign an IP address to a Connexium 499NOS17100 switch?
Title
Assign an IP address to a Connexium  499NOS17100

Issue
Assign an IP address to a Connexium  499NOS17100

Product Line
Connexium

Environment
Connexium

Cause
N/A

Resolution
To set the IP address, you will need to connect to the V24 port. See page 33.
Attached below is the manual for the 499NOS17100.

Schneider Electric Global

Attachment(s)
499NOS17100_manual.zip [1.53 MB]