undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV212- customer wants to monitor the fan so it will set an alarm in their Modbus register to let them know the fan is not running, before the drive faults
Issue:
Set Alarm for Modbus Register.

Product Line:
ATV212

Environment:
Modbus

Cause:
n/a

Resolution:
There is a Flashing L in the drive. This is to let you know you are getting close to a overheating fault. You can monitor this parameter ( FC91- register 64,657, bit 3 is the motor overload alarm).

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: